This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

about ccsv5 license

 If I get the " Node Locked Single User (N01D)" license, I can use it in two computers?
I may in the future expand it to floating license?
Is posible get the floating license via e mail like "Node Locked" license ? How much time I have to wait for receive it?

  • Hi Daniel,

    yes, you can input two MAC address and use a node locked license on two pcs (just not at the same time of course).   I do not believe changing license types is encouraged so I would try to be confident in which type is best for you.   I do believe a floating license comes via email as well.

    http://processors.wiki.ti.com/index.php/Licensing_-_CCS

    http://processors.wiki.ti.com/index.php/License_Server_Administration_for_CCS

    These wikis should also help.

    Best Regards,

    Lisa