This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear experts!
I have newly installed ccsv5.2.1,and I wanted to create 8 platforms for C6678 each core!
But It seems that there is something wrong with the new version of CCS,then I re-installed version CCSv5.2.0,which can work properly in the past,The problem appears either.
1 first i select menu "new" to create a new platform.
2 import standard 6678 configuration
3 click finish
4 It finishes successfully.
5 but When i want to edit it ,error occurs!
It always displays" Need to select platform package"
I can not proceed with the edit operation!
many thanks