This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiling VOLIB for C55 under CCS5.3



Hello:

I am trying to build volib_C55_2_0_0_3 with CCS5.3.  I am following the directions in the VOLIB: CCS Project Conversion ( prj_convert.html).

I have overcome the first obstetrical in getting a error message....  

**** Build of configuration Debug for project VOLIB_C55_PROJECT_CONVERT ****

C:\ti\ccsv5\utils\bin\gmake CCSVERSION=CCSV5 -k .projects

"C:\\ti\\ccsv5\\utils\\bin\\gmake" CCSVERSION=CCSV5 -k .projects
Cannot run program "C:\ti\ccsv5\utils\bin\gmake": The directory name is invalid.

I changed Build location -> Build directory: from its default of ${BuildDirectory}    to   ${workspace_loc:/VOLIB_C55_PROJECT_CONVERT} by pressing the Workspace... button.

That got rid of the error..

Now I get

**** Build of configuration Debug for project VOLIB_C55_PROJECT_CONVERT ****

"C:\\ti\\ccsv5\\utils\\bin\\gmake" CCSVERSION=CCSV5 -k .projects
gmake: Nothing to be done for `.projects'.

**** Build Finished ****

And of course the project is not converted...

Please help or tell me what I may be missing hear??

Thanks

Brian

  • Brian,

    I found out for each component (e.g TDU or CID), there are two projects under the packages (CID as an example):

    1) The first is under C:\ti\volib_c55_2_0_0_3\packages\ti\mas\cid\test. The project name is called like TI_MAS_CID_TEST_PROJECT_CONVERT. If I imported this into CCSV5.3, I met the issue you mentioned when clean/build.

    2) The other is deeper. It is under C:\ti\volib_c55_2_0_0_3\packages\ti\mas\cid\test\ccsProjects\test_rel_c5510_C55L_COFF. The project name is called like test_rel_c5510_C55L_COFF. If I imported this into CCSV5.3, I had no problem to clean/build.

    I hope you can resolve the issue with the second project.

    Regards, Eric