This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I'm building my project with either the full CCS environment (my development environment) or with the command line scripts (like explained on http://processors.wiki.ti.com/index.php/Projects_-_Command_Line_Build/Create --> that's my build machine environment)
Hi Stephane,
Stephane Mainier said:In order to make sure the developper using CCS always use the correct configuration (without the AUTOMATED_BUILD variable), I also want to limit me to a single configuration in this project.
One of the main purposes of supporting multiple build configurations is for use cases as yours where you wish to easily maintain build options. But I understand you wish to avoid this so:
Stephane Mainier said:So the question is: is there a way, during the import or the build done with the command line scripts, to automatically define my extra pre-defined macro?
Not by default with the command line build utility. If you want to add a preprocessor define variable outside the CCS environment before you build, you can try modifying the .*project files directly or define it in an options file that get included in the build. The options file is basically a text file which has additional build options. You can manually add/remove "--define=AUTOMATED_BUILD". This method is probably easier to deal with.
If I think of any more suggestions, I'll let you know.
Thanks
ki
The options (or command) file is basically a text file which has additional build options that is read by the compiler. The file is passed to the compiler via the flag:
--cmd_file=filename
For more information, see Section 2.3.2 of the Compiler User's Guide:
http://downloads.ti.com/docs/esd/SPNU151/index.html
To use it in CCS, use the field in the project properties as shown below:
Thanks
ki