This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
offline installation, antivirus disabled.
during installation this show up:
after click close button:
2867.60556FE5-C1A1-4061-8DF8-FFB8393BAE2D.rar
But ccs 5.3 installation is ok.
Hi Jianjun,
This crash seems to be related to an MS update on NVidia drivers for windows 7, 64 bit machines.
There are many complaints on the web and some solutions. One suggests that this may have something to do with the switching between the two display adapters not working.
As a workaround, could you go into NVidia Control Panel/3D Settings/Manage 3D settings, then for the "Base profile" Global presets, set Preferred graphics processor drop-down to "High-performance NVIDIA processor" if it was set on "Auto-select"?
Please let me know if this is fixes your issue.
Danish
Do you have an NVidia video adapter? Please see my previous post.
Thanks
Danish
Hi Jianjun,
please see my colleague Danishs' advice and keep us informed.
Best Regards,
Lisa
yes. your suggest may be right! the progress already pass previous fail point!
Installation completed! Hug you both! thanks!
Try this tormorrow with ccs 5.4 in office. http://e2e.ti.com/support/development_tools/code_composer_studio/f/81/t/276470.aspx
Hi Jianjun,
great, very happy to hear. All the best with development.
Thanks Danish!
Best Regards,
Lisa