This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I want to create a new CCS project for running on DM8168 EVM. But I can not find "TMS320DM8168" or any similar item to choose.
How should I select ?
Best Regards,
Michael Yu
Hi,
Did you update the software? Try custom updating the software.
Regards,
Gautam
Hi Gautam ,
I did the update of the CCS 5. But there was still not DM816x or any similar one for the DM8168 chip.
I don't know which device should be chosen for a new CCS project running on DM8168 evm.
Best Regards,
Michael
The screenshot in your first post shows a older version of CCS. Is that CCSv4? In any case it is good you followed Gautam's suggestion to update to v5. v5 should have this support. Perhaps you did not scroll down enough in the list. Also try typing in "DM816" in the search filter field to the left of the list. It should be there.
Thanks
ki
You may be using CCSv5, but you are using a very old version of v5. You are actually using v5.0, which I can tell because I can see "helios" in the Eclipse splash screen, which is Eclipse 3.6. CCSv5.0 was a limited release for a select number of devices. Please update to the latest version (currently 5.4.0)
thanks
ki