This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am using Olimex Header Board MSP430F1232 but I cannot download the programm or debug. With IAR it works but it is restricted to 4kb. Did Texas instruments test this adapter?
Regards, Tobias
I have an Olimex programmer here with me and I got it working with CCSv4.
Couple of things to look out for:
1. When installing CCSv4, there is an option in the installer that allows you to install Parallel Port Drivers for MSP430. You would need to select that.
2. Supports 4-wire JTAG mode only.
3. Inside your CCXML file, you would need to select "TI MSP430 LPT1" as your Connection programmer.
Regards,
William
Hello,
now i still have the problem with Olimex LPT and Code Composer 4.1.2.
COULD it PERHAPS be POSSIBLE that TI tests it´s software on their SIDE?
Thread MAIN DISCONNECTED
Error connecting to the target: No MSP430 device was found on LPT FET 1
IAR works on the same computer
Regards, Tobias