This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
When installing, I get the following error message.
Install Verification:
Installer failed to install com.ti.cgt.c6000.7.4.win32 correctly.The 2 most common reasons for failure are:
1: Anti-virus on your computer could have impeded the executable.
2. Download is corrupted.
The install log ends with the following:
03/18/2014 15:57:17PM - Executing Command Line: "D:/ti/ccsv5/eclipse/downloads/ti_cgt_c6000_7.4.4_setup_win32.exe" --mode silent --prefix "D:/ti/ccsv5/tools/compiler/c6000_7.4.4"
03/18/2014 15:57:20PM - Watching progressive output for matches
03/18/2014 15:57:21PM - ExternalProgramResult: child process exited abnormally
03/18/2014 15:57:21PM - ExternalProgramStatus: 1
03/18/2014 15:57:21PM - Externalprogramresult: child process exited abnormally
03/18/2014 15:57:21PM - state = feature registered
so,could you give me some suggestions to slove the question?
Hi,
So are your antivirus and firewall deactivated? Also, try downloading the offline setup again. Do keep us informed.
Regards,
Gautam
Hi,
in addition to Gautams advice, could you send the install logs? These are in the installjammer registry directory which may be hidden and is under program files or program files (x86).
Another thing to consider, noting a D drive is connection between two drives can sometimes be flaky/cause corruption. Can you try all locally?
Best Regards,
Lisa
Hi,
just thought to check for updates/installation logs.
Best Regards,
Lisa
Hi Pengfei,
happy to hear. Thanks for the update and all the best with development.
Best Regards,
Lisa