This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS: CCS5.5 Installation Fail

Tool/software: Code Composer Studio

I am attempting to install version CCS5.5.0.00077 and I am unable to get it to run. Please note that some file paths may contain typos in the log because the .exe was being ran from a network share. 

  • Hi Brandon,

    What version of Windows are you running (note that CCSv5.5 is not supported on Windows 10)?

    Also, why are you installing CCSv5.5? It is an unsupported version. I would only recommend it if you are using DSP/BIOS or using the old C54x device.

    Thanks

    ki

  • Hi Ki,

    It is being ran on Win7 x64. The reason I am trying to do CCS 5.5 is because there is still a need for it because its being used in support of Legacy devices.

    -Brandon

  • Brandon,

    Can you confirm that you are installing in a clean (empty) directory? If not, can you try installing in an empty directory?

    Thanks

    ki

  • Ki,

    I installed initially, and received the errors:

    1. Anti-Virus may be blocking the installer

    2. Download may be corrupt

    So I cleaned up all the directories it uses and deleted them, I uninstalled the AV software, and when I ran the next install, it was "Run as Administrator" and the directory was set to be C:\tinew based on the recommendation of another thread I saw as a troubleshooting step. 

    Thank you,

    Brandon

  • Ok, thanks.

    You mentioned that you were running the exe from a network share. To clarify, the install exe is not local to your machine but being run remotely?

  • Ki,

    I did initially run it from a share, and then I transferred all the installer files locally and attempted again and it produced the same log file. 

    -B

  • Can you post your latest install log files?

    Thanks

    ki

  • Ki,

    Please find the updated log file. 

    5700.0763.ccs_setup_5.5.0.00077_install.log

  • Thanks. Our installer expert has analyzed the logs and it appears that you are running into a known installer issue with one of the components. Normally a clean reinstall resolves the issue but clearly this is not happening in your case. We don't have a good solution for this other than updating to a later CCS version. If you must use CCSv5.5, there may be some other workaround that could work for you. Please start a private conversation with me to discuss further.

    Thanks

    ki

  • Hello,
    I haven’t heard back from you, hence this issue is being closed. If you wish to continue the discussion, please post a reply with an update below (or create a new thread).

    Thanks,
    ki

  • Thank you for following up, I've sent a message to you for further discussion. 

    -Brandon

  • Thanks Brandon,

    I'll follow up with you via PM.

    ki