Hi,
I was wroking with CCS3.3 and migrated the project to CCS4 (4.0.0.16000 ) 32K MCU Core Edition. Target is F2812. I could build the project in CCS4 with minor compiler warnings, following the guidelines from the web.
I want to (1) Simulate the project with simulator and (2) Debug with SPI515PP JTAG Emulator from Spectrum Digital.
Problem with (1): I tried to create a new (User Defined) Target Configuration file. But I could not find a suitable 'Connection Type' and 'Device' option for F2812. Please guide to properly configure target to simulate the project for F2812.
Problem with (2): While creating Target Configuration file, which 'Connection Type' and 'Device' option to choose for F2812 and SPI515PP Emulator?. Does the driver for SPI515PP Emulator comes along with CCS4 installer?. Please help to debug F2812 with SPI515PP Emulator.
My PC is having on 256MB RAM. Is it causing any problem?
Any help is greately appreciated!
-Sinoj