Hi,
I am using CCSv4 version 4.0.0.16000 with code gen toools 6.1.9.
I have one project created with these tools and now I want to build the same project with cgt v6.1.13 from the same ccs version.
Is there a way to specify code gen tool version tool to be used to build a project other than than the one used for creating the project?
Or is the only option is to modify the project itself?
Meena