So I looked at the other threads that come up with this title. They are no help.
Here is the error I get in CCSv6 while debugging:
Can't find a source file at "/db/vtree/library/trees/zumaprod/zumaprod-a23/tirtos_tivac_2_00_01_23/products/ndk_2_23_01_01/packages/ti/ndk/stack/fdt/fileuser.c"
It is obvious that the problem is that the file path embedded in the NDK library was compiled with the path above. I have done a normal TI RTOS install with the path to file being:
C:\ti\tirtos_tivac_2_00_01_23\products\ndk_2_23_01_01\packages\ti\ndk\stack
The real problem is that clicking the "Locate File..." button does *not* get the debugger to find the path to the file. What is worse, is that it now can't find the path to *my* source file after navigating to the directory for the NDK file.
The only solution at this point is to rebuild the library so that the local library has the correct path names. I would really prefer to be trying to find out why my call to fdSelect causes my program to exit!!!
Can you add an urgent request to the debugger team to fix this problem?
Thanks.
Ray