This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
So i decided to try out the c2000 launchpad. I had alreddy installed CCS before but i only installed the files for Tiva and MSP430. Now i am trying to use CCS with the C2000 but i can't find the device when i try to create a project.
Am i doing something wrong? I can't find a way to update CCS to have C2000 compiler
Hi Luis,
You will need to install device support for C2000. One way to do this is to re-reun the CCS installer you use to originally install CCS, and select the same install directory. The installer will detect that there is an existing CCS install in there and allow you to modify the existing install (add/remove). For here you can select the options to add C2000 support.
Thanks
ki
Unfortunately it seems that isn't possible for CCS V6. it asks me to use check for updates but i don't see anything for the C2000 there.
I checked and i have some of the C2000 but nothing of the family of the launchpad (and probably other ones missing too)