This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I have install CCSv6 with following processor configuration. After installing I am not able to create project..
My CCS version is 6.
operating system: windows 7
In create new project window file menu ->New -> CCS project. I see following device:
2, When i try to browse a examples. following window occur, not able to see any example.
So please any one tell how to start working with especially for EVM.
is there any dependency that i require to install?
Thanks,
Rahul Tiwari
Rahul,
The screen captures did not come through. I installed the latest keystone package from the update manager and I am able to create projects ok for this device. Where are you trying to browse for examples? CCS doesn't come with any examples for this device other than the very basic templates in the project wizard. Are these TI-RTOS examples? Are these examples from an SDK? If you can let me know I can help connect you with someone to help.
Regards,
John