Other Parts Discussed in Thread: MSP430F5438A
hello,
i used the msp430f5438A.
and CCS 5.3.
and compiler version:TI v4.1.2
and i run in mclk = 16mhz.
Is there any documentation that provides data
about floating point emulation performance?
thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: MSP430F5438A
hello,
i used the msp430f5438A.
and CCS 5.3.
and compiler version:TI v4.1.2
and i run in mclk = 16mhz.
Is there any documentation that provides data
about floating point emulation performance?
thanks.
float/double operation taking too long.
e.g.
my system time build in that way:
typedef time_t double;
time_t systemtime;
#define Tick 0.0001; // the clock is 10khz ,
//hence every 0.0001sec i promoting the time
and in the time interrupt service routine i write:
systemtime += Tick;
this simple operation of :
systemtime += Tick;
take about 60usec ( i measure it by scope).
and because i run in 16mhz , in mean the the number of assembly operation for
making this simple operation is 16 * 60 = 960 cycles or
about 960 assembly commands.
1) Is the result I got is reasonable?
2)second thing:
I would like to receive information
about the number of cycles of simple operations like
multiplication, addition, subtraction, division.
Is this information exist?
thanks.
There isn't any rigorous profiling of the basic operations, but you should expect something on the order of the following.
IEEE-32 IEEE-64
add 174 737
sub 177 794
mul 372 1355
div 408 4387
I strongly suggest you use "unsigned long long" instead of a floating-point type to maintain a counter.