This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I've searched through the forums and found many posts regarding App Center and how it fails to work. I've tried all of the suggestions with no luck. I am able to update CCS whenever it is required.
Specifically, I am trying to install TI-RTOS for TivaC. I have installed Code Composer Studio Version: 6.1.0.00104 on a Windows 7 machine. From the App Center I select TI-RTOS for TivaC and click on the Install Software button. The status bar on the bottom appears to get to a server but eventually I get the error message: Failed to install the selected add-ons. Please see the Error Log for more details.
The Eclipse Log:
!ENTRY com.ti.ccstudio.p2app 4 0 2015-04-20 14:04:46.767
!MESSAGE The installable unit ,com.ti.rtsc.TIRTOStivac.product.feature.group has not been found.
I was able to download the TI-RTOS from ti.com however I am reluctant to install it as the recommended procedure is to use the App Center. I have found CCS/Eclipse can be very fussy and I prefer to use the recommended installation if possible.
Robert
Thanks for helping.
I updated code composer on 4/16 with no issues. I can't download any add-on from the app center. I can download the non-add-on software like tivaware (clicking download directs me to a download site).
Robert
Robert Hoffman said:I updated code composer on 4/16 with no issues.
Did you have CCS 6.0.1 before applying this update? In other words, do you know if the update you did on 4/16 updated your CCS from 6.0.1 to 6.1.0?
I'm not sure. While trying to debug this problem, I uninstalled Code Composer and started with a fresh install. This was done on 4/16 from an install file I downloaded on 4/9. Also, I received an update alert when I started CCS this morning.
Robert Hoffman said:I can't download any add-on from the app center.
If you are not able to download any add-on from App Center it could have to do with your proxy settings. Please check your proxy settings. This wiki page may be helpful.
Not sure if this is helpful or not but I am getting prompted that there is a 'Debug Server Flash' update available when I start CCS. I can also click on Check For Updates and I get the same 'Debug Server Flash' available update.
Hi Robert,
Would you be able to try a different path to install TI-RTOS? You would need to start CCS and go to Help->Install New Software. When a dialog pops up, click on "Add" button in top right corner. In the dialog for Name enter "TI-RTOS for Tivac", the name does not really matter, but something relevant helps. Then in Location: field enter http://software-dl.ti.com/targetcontent/esd/tirtos_tivac/update/ Once you close the dialog you should see dialog like below. Check TI RTOS and click Next few times. The app center goes through a very similar process, but there is a very small layer on top of those manual step. Knowing whether it works with these manual steps would greatly to narrow down the problem area.
Thank you,
Martin