This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Import failed because its meta-data cannot be interpreted



Hello,

I have a project which is running fine in my existing workspace. But when I try to import it into a new clean workspace I get this warning:

See details below. 
  Error: Import failed for project 'PFC_SubSystem' because its meta-data cannot be interpreted. Please contact support.

This happens under linux and windows on my local machine, both running 6.1.0.00104 and also on my colleagues machine running windows with the same version. Another colleague also running this version windows does NOT have this problem.

Link to .ccsproject: http://pastebin.com/tTTVsuw7

Link to .cproject: http://pastebin.com/gxA8M5GN 

Link to .project: http://pastebin.com/EESpgYck 

Any help would be great.

Sincerely,

Sebastian