This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
When I try to download software to my target - I am getting this error:
Error connecting to the target:
(Error -242 @ 0x0)
A router subpath could not be accessed.
The board configuration file is probably incorrect.
(Emulation package 6.0.14.0)
I do not know where it came from. Day ago, everything was work without error.
I even tried to create completely new workspace, rebuild project - and same error occurred again.
What shall I do?
Hey,
we are currently encountering the same problem with the same error massage when trying to program the chip. Which pin alignment was faulty?
The Jtag connection? or probably the footprint on the PCB?
i hope you can help us, since this is almost 1 year old.
edit: Okay as i noticed the error message is not quite the same... we are getting:
Error connecting to the target: (Error -241 @ 0x0) A router subpath could not be accessed. A security error has probably occurred. (Emulation package 6.0.14.5)
greetings,
philipp
Hello Philipp,
have you solved the problem of Error connecting to the target:(Error-241@0x0). I am also facing same error.
I am waiting for a positive reply from your side.
Thanks in advance!
Hi,
I'm facing a similar problem.
I built a prototype using CC2640 and started to play with it, not paying much attention on the ESD and other little glitches that may occur while performing such debug tasks on an open circuit laying on the desk.
After couples days working fine, I now get an error message when trying to program the device:
Error connecting to the target:(Error -242 @ 0x0)
A router subpath could not be accessed.
The board configuration file is probably incorrect.
(Emulation package 6.0.228.0)
I do have a second prototype which I still can program with no problem (unfortunately I can't use that particular one for my testing)
Another important point, is hat the devpack I was using when the programming stopped working is now dead (no more recognized as a USB device). It was an old rev 1.2.0 one.
I suspect something wrong in the JTAG connection, since everything is working fine on the CC2640. Just, I'm no more able to upload a new firmware.
Is there something particular I should check before trying to replace the unit (since this is not an easy task!)
Thanks
JYL
Hello Mehmet,
I'm really glad you posted this answer, because I have been tearing my hair out for almost a week working on this. I am attempting to port a BLE STACK 2.0 project to 2.2.1, and in the process an update to CCS upgraded the firmware on my XDS110 debugger. This in turn apparently reset the jTAG connection mode and prevented me from loading code on to my custom board that had previously been working perfectly fine.
I know this probably isn't the proper forum, but shame on TI for changing settings like this on a software upgrade! I completely blew out my TI CCS installation, reinstalled everything, and really hoped that would solve my problem, but it didn't. It took scouring the forums to find someone nice like Mehmet that had the same problem in order for me to fix it. I know TI has a tough job supporting so many microcontrollers from a single IDE, but my entire experience with CCS and the code breaking changes on every upgrade of BLE STACK has really made me reconsider their products.
If I had the choice in the future, I'd stay far away from TI and CCS if it were up to me.
Anyways, thanks Mehmet!
-Ben
Hello
now I had met the same problem as you
could you give me some explanation of pin alignment? I dot not understand this.
Thank you in advance.
BRS,
Meng