This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TI cloud IDE installation for ti cloud

Other Parts Discussed in Thread: ENERGIA

Session ID: 1438191151566_00001550

I logged in to use the TI cloud dev tools for my MSP432 board, since i cannot get CCS 6.1 to work ( posted about that earlier).

There is mention of the need for the TI cloud bridge, but i do not know where to get that to install, and does not show up in my google chrome extensions.

My OS is windows 7  professional 64-bit, running google chrome Version 44.0.2403.155 m (64-bit)

  • Hi David,
    You should be able to just select your project and then click "Flash" or "Debug" buttons. If cloud agent (bridge) is not installed then you should get pops up asking you to install them.

    Martin
  • Works. Thanks. I however get another issue where i get a flash load failure for the resource explorer msp-exp432p401r out of the box experience and blink led. I have not tried any other examples.
  • Hi David,
    Could you let us know what type of an error you are getting? Are you using a MSP432 launchpad?

    Thanks,
    Martin
  • Running windows 7 professional  64-bit  on an AMD A6-5400 cpu and 4GB ram machine.

    Now i am trying to run the 'blink.' energia project on the MSP432P401R launchpad development kit

    1)- When i click the 'flash' button, project builds ok, but i get the following error message:

    Flashing failed!

    Installation failed : An unknown error occure : Invalid or unsupported

    zip format. No END header found.

    2)- When i select  Target-> Connect Comm port from the main menu,

    I get a pop up box with the following message:

    Opening COM port failed!

    Installation failed: An unknown error occured: Error: rad

    ECONNRESET.

    In the windows device manager i have the following listed when the board is connected to my PC:

    XDS110 Class Application/User UART (COM5)

    XDS110 Class Auxiliary Data Port (COM6)

  • David,

    Can you grab the log file from %USERPROFILE%\ti\node\TICloudAgent.log

    Thanks,
    Mandeep
  • TICloudAgent.log
    Fullscreen
    1
    2
    3
    4
    5
    6
    7
    8
    9
    10
    11
    12
    13
    14
    15
    16
    17
    18
    19
    20
    21
    22
    23
    24
    25
    26
    27
    28
    29
    30
    31
    32
    33
    34
    35
    36
    37
    38
    39
    40
    41
    42
    43
    44
    45
    46
    47
    48
    49
    50
    51
    52
    53
    54
    55
    56
    57
    58
    59
    60
    61
    62
    63
    64
    65
    66
    67
    2015-08-14T21:06:27.649Z - info: Overridden Proxy = source=unknown
    2015-08-14T21:06:27.652Z - info: Creating db dir : C:\Users\dnyarko\AppData\Local\TEXASI~1\TICLOU~1\db source=unknown
    2015-08-14T21:06:27.652Z - info: Creating loaders dir : C:\Users\dnyarko\AppData\Local\TEXASI~1\TICLOU~1\loaders source=unknown
    2015-08-14T21:06:27.653Z - info: Could not open installed.json : Error: ENOENT, no such file or directory 'C:\Users\dnyarko\AppData\Local\TEXASI~1\TICLOU~1\db\installed.json' source=unknown
    2015-08-14T21:06:27.653Z - info: Could not open targets.json : Error: ENOENT, no such file or directory 'C:\Users\dnyarko\AppData\Local\TEXASI~1\TICLOU~1\db\targets.json' source=unknown
    2015-08-14T21:06:27.657Z - info: Getting Component Info: http://dev.ti.com/ticloudagentinstaller/getComponentInfo?component=xds110_drivers source=unknown
    2015-08-14T21:06:27.657Z - info: Looking up proxy settings for url http://dev.ti.com source=unknown
    2015-08-14T21:06:27.895Z - info: Setting proxy to source=unknown
    2015-08-14T21:06:27.895Z - info: installer.js using proxy: source=unknown
    2015-08-14T21:06:28.206Z - info: Looking up proxy settings for url http://dev.ti.com source=unknown
    2015-08-14T21:06:28.258Z - info: Setting proxy to source=unknown
    2015-08-14T21:06:28.258Z - info: installer.js using proxy: source=unknown
    2015-08-14T21:06:28.259Z - info: Get: http://dev.ti.com/ticloudagentinstaller/getComponent?os=win&component=xds110_drivers source=unknown
    2015-08-14T21:06:28.454Z - info: Response: 200 source=unknown
    2015-08-14T21:06:28.454Z - info: Saving to temporary location: C:\Users\dnyarko\AppData\Local\Temp\ticloudagent_artifacts\xds110_drivers.zip source=unknown
    2015-08-14T21:06:36.978Z - info: Running command : C:\Users\dnyarko\TICloudAgent\drivers\dpinst_64_eng.exe /path C:\Users\dnyarko\AppData\Local\Temp\ticloudagent_artifacts\xds110_drivers\xds110_drivers /c /SW /SA source=unknown
    2015-08-14T21:08:07.190Z - info: RetCode = 512 source=unknown
    2015-08-14T21:08:07.190Z - info: DPInst Run Successfully Ret Code: 0x200 source=unknown
    2015-08-14T21:08:07.194Z - info: Added to Installed Components DB:xds110_drivers source=unknown
    2015-08-14T21:13:55.070Z - info: Staring directory : C:\Users\dnyarko\TICLOU~1\src source=unknown
    2015-08-14T21:13:55.071Z - info: Starting Agent! source=unknown
    2015-08-14T21:13:55.080Z - info: Module( Agent )->Web socket server started! source=unknown
    2015-08-14T21:13:55.082Z - info: Discovered Module : DS source=unknown
    2015-08-14T21:13:55.085Z - info: Discovered Module : File source=unknown
    2015-08-14T21:13:55.087Z - info: Discovered Module : Flash source=unknown
    2015-08-14T21:13:55.144Z - info: Discovered Module : Serial source=unknown
    2015-08-14T21:13:55.154Z - info: Discovered Module : TargetSupport source=unknown
    2015-08-14T21:13:55.154Z - info: len= source=unknown
    2015-08-14T21:13:55.155Z - info: <Buffer 1e 00 00 00> source=unknown
    2015-08-14T21:13:55.155Z - info: buf= source=unknown
    2015-08-14T21:13:55.155Z - info: <Buffer 7b 22 70 6f 72 74 22 3a 35 35 34 39 39 2c 22 76 65 72 73 69 6f 6e 22 3a 22 32 2e 32 22 7d> source=unknown
    2015-08-14T21:13:55.241Z - info: Module( Agent )->Exec Command : listCommands:1 source=unknown
    2015-08-14T21:13:55.242Z - info: Module( Agent )->Ret Command ( response) : listCommands : 1 source=unknown
    2015-08-14T21:13:55.253Z - info: Module( Agent )->Exec Command : addConfigProperty:2 source=unknown
    2015-08-14T21:13:55.253Z - info: Setting property cloudAgentInstallerServerURL : http://dev.ti.com/ticloudagentinstaller source=unknown
    2015-08-14T21:13:55.253Z - info: Module( Agent )->Ret Command ( response) : addConfigProperty : 2 source=unknown
    2015-08-14T21:13:55.611Z - info: Module( Agent )->Exec Command : createSubModule:3 source=unknown
    2015-08-14T21:13:55.611Z - info: Module( Agent )->Creating Sub Module : File source=unknown
    2015-08-14T21:13:55.613Z - info: Module( File )->Web socket server started! source=unknown
    2015-08-14T21:13:55.614Z - info: Module( Agent )->Ret Command ( response) : createSubModule : 3 source=unknown
    2015-08-14T21:13:55.622Z - info: Module( File )->Exec Command : listCommands:1 source=unknown
    2015-08-14T21:13:55.622Z - info: Module( File )->Ret Command ( response) : listCommands : 1 source=unknown
    2015-08-14T21:13:55.871Z - info: Module( File )->Exec Command : write:2 source=unknown
    2015-08-14T21:13:55.873Z - info: Module( File )->Ret Command ( response) : write : 2 source=unknown
    2015-08-14T21:13:55.876Z - info: Module( Agent )->Exec Command : createSubModule:4 source=unknown
    2015-08-14T21:13:55.876Z - info: Module( Agent )->Creating Sub Module : TargetSupport source=unknown
    2015-08-14T21:13:56.395Z - info: Overridden Proxy = source=unknown
    2015-08-14T21:13:56.436Z - info: Could not open targets.json : Error: ENOENT, no such file or directory 'C:\Users\dnyarko\AppData\Local\TEXASI~1\TICLOU~1\db\targets.json' source=unknown
    2015-08-14T21:13:56.442Z - info: Module( TargetSupport )->Web socket server started! source=unknown
    2015-08-14T21:13:56.442Z - info: Module( Agent )->Ret Command ( response) : createSubModule : 4 source=unknown
    2015-08-14T21:13:56.448Z - info: Module( TargetSupport )->Exec Command : listCommands:1 source=unknown
    2015-08-14T21:13:56.449Z - info: Module( TargetSupport )->Ret Command ( response) : listCommands : 1 source=unknown
    2015-08-14T21:13:56.454Z - info: Module( TargetSupport )->Exec Command : add:2 source=unknown
    2015-08-14T21:13:56.455Z - info: Getting Install Info: http://dev.ti.com/ticloudagentinstaller/ticloudagentinstaller/getInstallInfo?os=win&deviceID=msp432p401r&connectionID=TIXDS110_Connection source=unknown
    2015-08-14T21:13:56.455Z - info: Looking up proxy settings for url http://dev.ti.com/ticloudagentinstaller source=unknown
    2015-08-14T21:13:56.492Z - info: Setting proxy to source=unknown
    2015-08-14T21:13:56.493Z - info: installer.js using proxy: source=unknown
    2015-08-14T21:13:56.663Z - info: Additional packages need to be installed to support C:\Users\dnyarko\AppData\Local\Temp\ti_cloud_storage\MSP432P401R.ccxml. Starting Install Process.
    source=unknown
    2015-08-14T21:13:56.663Z - info: Installing Components: [{"DSLite":{"type":"files","path":"loaders","name":"DSLite"},"xds110_drivers":{"type":"windriver","name":"xds110_drivers"},"MSP432":{"type":"files","path":"loaders","name":"MSP432"}}] source=unknown
    2015-08-14T21:13:56.663Z - info: Installing package : DSLite
    source=unknown
    2015-08-14T21:13:56.663Z - info: Looking up proxy settings for url http://dev.ti.com/ticloudagentinstaller source=unknown
    2015-08-14T21:13:56.701Z - info: Setting proxy to source=unknown
    2015-08-14T21:13:56.701Z - info: installer.js using proxy: source=unknown
    2015-08-14T21:13:56.702Z - info: Get: http://dev.ti.com/ticloudagentinstaller/ticloudagentinstaller/getComponent?os=win&component=DSLite source=unknown
    2015-08-14T21:13:56.865Z - info: Response: 200 source=unknown
    XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

    File inserted

  • David,

    Can you please check the size, date modified/created of C:\Users\dnyarko\AppData\Local\Temp\ticloudagent_artifacts\DSLite.zip. It looks like the downloaded file is corrupted. Can you also try to unzip ( double click in windows ) it to see if it opens.

    Also,
    What happens when you try the same action again?

    Thanks,
    Mandeep
  • File size is 1kb, date modified is 17th August 2015 at 2:35pm.

    When i try to open it, i get an 'invalid file' message.

    How  do i go about re-downloading it.

    Thanks

  • Can you please attach the file (DSLite.zip).
    As with regards to re-downloading. It should automatically try to do it. But, just to be sure.. can you delete %LOCALAPPDATA%\Texas Instruments\TICloudAgent\db and %LOCALAPPDATA%\Texas Instruments\TICloudAgent\loaders folder and try to flash again.

    Regards,
    Mandeep
  • I must be missing something. I cannot find an option to attach a file, only to insert a file, which does not work for the DSLite.zip file
  • Can you just open DSLite.zip in any text editor ( notepad ) and see if there is any useful info there.
  • I opened it with a text editor, found it had HTML headers so saved it as html and opened it with my browser. I have pasted the image below.

    Looks like the download was blocked by our Corporate firewall.

  • David,

    I am not sure why your firewall is blocking a request to dev.ti.com. 

    Can you see if you see if the request goes through via the browser. I am trying to see if I can narrow the problem down to our in-line installer. Try putting the following url into your browser and see if the firewall blocks that.

    http://dev.ti.com/ticloudagentinstaller/ticloudagentinstaller/getComponent?os=win&amp;component=DSLite

    Regards,
    Mandeep Deol

  • Looks like the link in the last reply is malformed. Trying again.

    "dev.ti.com/.../getComponent;component=DSLite"

  • On entering the link i get the following message in both Firefox and Google chrome:

    {message : missing paramater = component}

    Using Internet explorer 11, the message is : 'The webpage cannot be found
  • E2E is doing something odd with the link. When you paste it in your browser remove the "amp;" from the url.
  • Tried this. I now get the message:

    Ready to go!

  • David,

    Let's take this offline. I sent you friend request; please accept that so we can start an offline conversation.

    Regards,
    Mandeep Deol
  • Turned out that the David's corporate firewall was blocking download requests from ti.com; which blocks cloud agent from downloading the appropriate device support files. An exception needs to be added to the firewall policy.