It seems to have problems loading C:/ti/uniflash_3.4/eclipse/plugins/com.ti.uniflash.wireless.files_1.0.0.201509170706/cc3xxx/bin/win/FlashAPI.dll, but the file definitely exists and I can open it in notepad.
This is similar to issues reported in this forum previously, but the solutions posted in those threads did not work on my machine - one was for Windows XP and the other one crashed Uniflash when I tried running it with the posted DLL.
The solution posted in this thread crashed when I tried using it. It also was resolved by updating to 3.2, but I am having this problem on 3.4. This thread solved the issue for Windows XP. I ran Uniflash in compatibility mode with Windows XP and the problem still existed.
I have uninstalled and reinstalled Uniflash multiple times and the problem still persists. I have tried using regsvr to register the DLL in question, but it also failed with this error message:
"The module could not load. Make sure the binary is stored at the specified path or debug it to check for problems with the binary or dependent .DLL files. The specified module could not be found"
It seems that the issue is with the DLL itself, and is machine-specific.
Is there a way to revert my Uniflash to version 3.2 to test if this issue was reintroduced in 3.3/3.4? And if not, how do I proceed?