This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS hangs up (automatically exit) when drawing graph

Other Parts Discussed in Thread: MOTORWARE

Hello,

I would like to ask a question about using graph on CCS.

I tried to draw a graph of motor current on CCSv6 using "Instaspin lab 5b",but , CCS hangs up (automatically exit)

while debugging.

What I did to show graph is , right click on the motor current variable on watch window,and selected menu "graph",

and set it to continuous reflesh mode,and started debugging.

What should I do to prevent it and could watch the graph of motor current ?

 I would appriciate if someone could reply to my question.

Regards,

Hiroyasu

  • Hi Hiroyasu-san,

    Can you try using a ferrite core based USB cable? or simply wind the usb cable multiple times to an external ferrite core.
    Check for any improvement.

    Regards,
    Gautam
  • Hiroyasu Matsubara said:
    What I did to show graph is , right click on the motor current variable on watch window,and selected menu "graph",

    Have you tried opening the graph view using the main CCS Tools menu? Is the issue reproducible that way too?

    Does CCS hang (automatically exit) when viewing graphs for other projects as well or is it only for this project? The docs for Motorware provide a description/example of using graphs for proj_lab05f. Does that one work well?