Other Parts Discussed in Thread: MSP430FR4133
Greetings all;
I'm compiling the "Out Of Box MSP430FR4133" project and I get these errors:
BTW This list was shortened to remove duplicate error tags and all of them
repeat more then once..
>> WARNING: --near_data is only applicable for large data models. Option ignored.
"../StopWatchMode.c", line 127: remark #1530-D: (ULP 5.1) Detected modulo operation(s). Recommend moving them to RAM during run time or not using as these are processing/power intensive
"../StopWatchMode.c", line 158: remark #1530-D: (ULP 5.1) Detected divide operation(s). Recommend moving them to RAM during run time or not using as these are processing/power intensive
Finished building: ../StopWatchMode.c
>> WARNING: --near_data is only applicable for large data models. Option ignored.
"../TempSensorMode.c", line 53: warning #145-D: a value of type "volatile unsigned int *" cannot be used to initialize an entity of type "volatile int *"
"../TempSensorMode.c", line 129: remark #1527-D: (ULP 2.1) Detected SW delay loop using __delay_cycles. Recommend using a timer module instead
"../TempSensorMode.c", line 144: remark #1533-D: (ULP 6.1) Detected use of multiplication on a device that has no hardware multiplier
Finished building: ../TempSensorMode.c
>> WARNING: --near_data is only applicable for large data models. Option ignored.
"../hal_LCD.c", line 101: remark #1546-D: (ULP 15.1) Detected consecutive bitfield assigns. Recommend using bit mask instead
"../hal_LCD.c", line 141: remark #1544-D: (ULP 13.1) Detected loop counting up. Recommend loops count down as detecting zeros is easier
"../hal_LCD.c", line 147: remark #2553-D: (ULP 14.1) Array index (involving "t") of type "int". Recommend using "unsigned int"
"../hal_LCD.c", line 152: remark #1545-D: (ULP 14.1) Array index of type "int". Recommend using "unsigned int"
"../hal_LCD.c", line 163: remark #1527-D: (ULP 2.1) Detected SW delay loop using __delay_cycles. Recommend using a timer module instead
"../hal_LCD.c", line 140: remark #1535-D: (ULP 8.1) variable "buffer" is used as a constant. Recommend declaring variable as either 'static const' or 'const'
"../hal_LCD.c", line 152: remark #1545-D: (ULP 14.1) Array index of type "int". Recommend using "unsigned int"
"../hal_LCD.c", line 186: remark #2553-D: (ULP 14.1) Array index (involving "position") of type "int". Recommend using "unsigned int"
Finished building: ../hal_LCD.c
>> WARNING: --near_data is only applicable for large data models. Option ignored.
"../main.c", line 249: remark #1538-D: (ULP 10.1) ISR PORT1_ISR calls function RTC_start. Recommend moving function call away from ISR, or inlining the function, or using pragmas
"../main.c", line 251: remark #1538-D: (ULP 10.1) ISR PORT1_ISR calls function RTC_stop. Recommend moving function call away from ISR, or inlining the function, or using pragmas
"../main.c", line 260: remark #1538-D: (ULP 10.1) ISR PORT1_ISR calls function Timer_A_initUpMode. Recommend moving function call away from ISR, or inlining the function, or using pragmas
"../main.c", line 301: remark #1538-D: (ULP 10.1) ISR PORT2_ISR calls function resetStopWatch. Recommend moving function call away from ISR, or inlining the function, or using pragmas
Finished building: ../main.c
>> WARNING: --near_data is only applicable for large data models. Option ignored.
"../driverlib/MSP430FR2xx_4xx/cs.c", line 427: remark #1535-D: (ULP 8.1) variable "dco_FLLD" is used as a constant. Recommend declaring variable as either 'static const' or 'const'
Finished building: ../driverlib/MSP430FR2xx_4xx/cs.c
>> WARNING: --near_data is only applicable for large data models. Option ignored.
"../driverlib/MSP430FR2xx_4xx/eusci_a_uart.c", line 56: remark #1535-D: (ULP 8.1) variable "retVal" is used as a constant. Recommend declaring variable as either 'static const' or 'const'
"../driverlib/MSP430FR2xx_4xx/eusci_a_uart.c", line 122: remark #1528-D: (ULP 3.1) Detected flag polling using UCTXIFG. Recommend using an interrupt combined with enter LPMx and ISR
Finished building: ../driverlib/MSP430FR2xx_4xx/eusci_a_uart.c
>> WARNING: --near_data is only applicable for large data models. Option ignored.
"../driverlib/MSP430FR2xx_4xx/eusci_b_i2c.c", line 208: remark #1528-D: (ULP 3.1) Detected flag polling using UCTXIFG. Recommend using an interrupt combined with enter LPMx and ISR
"../driverlib/MSP430FR2xx_4xx/eusci_b_i2c.c", line 541: remark #1527-D: (ULP 2.1) Detected SW delay loop using empty loop. Recommend using a timer module instead
Finished building: ../driverlib/MSP430FR2xx_4xx/eusci_b_i2c.c
>> WARNING: --near_data is only applicable for large data models. Option ignored.
<Linking>
warning #10420-D: For FRAM devices, at start up, the GPO power-on default high-impedance mode needs to be disabled to activate previously configured port settings. This can be done by clearing the LOCKLPM5 bit in PM5CTL0 register.
remark #10205-D: automatic RTS selection: linking in "rts430_eabi.lib" in place of index library "libc.a"
remark #10372-D: (ULP 4.1) Detected uninitialized Port A in this project. Recommend initializing all unused ports to eliminate wasted current consumption on unused pins.
remark #10372-D: (ULP 4.1) Detected uninitialized Port B in this project. Recommend initializing all unused ports to eliminate wasted current consumption on unused pins.
remark #10372-D: (ULP 4.1) Detected uninitialized Port C in this project. Recommend initializing all unused ports to eliminate wasted current consumption on unused pins.
remark #10372-D: (ULP 4.1) Detected uninitialized Port D in this project. Recommend initializing all unused ports to eliminate wasted current consumption on unused pins.
Finished building target: OutOfBox_MSP430FR4133.out
I realize that the (ULP) is for the Ultra Low Power adviser. So my question is how do I assign these
variable to different areas of ram to satisfy the ULP?
Also is there a reference for all of the warning and error codes that can be produced by the compiler
and linker?
BTW don't advise about the ">> WARNING: --near_data is only applicable for large data models. Option ignored." I already know what caused that.
Thanks J.B.G.