This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I am using window 10 pc and cc2650stk.
I have used CCS 6.1.2, BLE stack 2.1.1 , TI RTOS 2.13.0.06, XDCtool 3.31.3.33, Compiler version TI v5.2.5. for following log.
I am getting following activity log after building example project of sensor tag from ble stack.
**** Build of configuration FlashOnlyOAD for project SensorTag ****
"C:\\ti\\ccsv6\\utils\\bin\\gmake" -k all
'Building file: C:/ti/simplelink/ble_cc26xx_2_01_01_44627/Projects/ble/SensorTag/CC26xx/CCS/Config/appBLE.cfg'
'Invoking: XDCtools'
"C:/ti/xdctools_3_31_01_33_core/xs" --xdcpath="C:/ti/tirtos_simplelink_2_13_00_06/packages;C:/ti/tirtos_simplelink_2_13_00_06/products/bios_6_42_00_08/packages;C:/ti/tirtos_simplelink_2_13_00_06/products/uia_2_00_02_39/packages;C:/ti/ccsv6/ccs_base;" xdc.tools.configuro -o configPkg -t ti.targets.arm.elf.M3 -p ti.platforms.simplelink:CC2650F128 -r release -c "C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.5" --compileOptions "-mv7M3 --code_state=16 --abi=eabi -me --include_path=\"C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.5/include\" --include_path=\"C:/ti/simplelink/ble_cc26xx_2_01_01_44627/Projects/ble/SensorTag/CC26xx/Source/Application\" --include_path=\"C:/ti/simplelink/ble_cc26xx_2_01_01_44627/Projects/ble/include\" --include_path=\"C:/ti/simplelink/ble_cc26xx_2_01_01_44627/Projects/ble/ICall/Include\" --include_path=\"C:/ti/simplelink/ble_cc26xx_2_01_01_44627/Projects/ble/Profiles/Roles/CC26xx\" --include_path=\"C:/ti/simplelink/ble_cc26xx_2_01_01_44627/Projects/ble/Profiles/Roles\" --include_path=\"C:/ti/simplelink/ble_cc26xx_2_01_01_44627/Projects/ble/Profiles/Keys\" --include_path=\"C:/ti/simplelink/ble_cc26xx_2_01_01_44627/Projects/ble/Profiles/DevInfo\" --include_path=\"C:/ti/simplelink/ble_cc26xx_2_01_01_44627/Projects/ble/Profiles/SensorProfile/cc26xx\" --include_path=\"C:/ti/simplelink/ble_cc26xx_2_01_01_44627/Projects/ble/Profiles/OAD/cc26xxST\" --include_path=\"C:/ti/simplelink/ble_cc26xx_2_01_01_44627/Projects/ble/common/cc26xx\" --include_path=\"C:/ti/simplelink/ble_cc26xx_2_01_01_44627/Components/applib/heap\" --include_path=\"C:/ti/simplelink/ble_cc26xx_2_01_01_44627/Components/ble/hci\" --include_path=\"C:/ti/simplelink/ble_cc26xx_2_01_01_44627/Components/ble/controller/CC26xx/include\" --include_path=\"C:/ti/simplelink/ble_cc26xx_2_01_01_44627/Components/ble/host\" --include_path=\"C:/ti/simplelink/ble_cc26xx_2_01_01_44627/Components/hal/target/CC2650TIRTOS\" --include_path=\"C:/ti/simplelink/ble_cc26xx_2_01_01_44627/Components/hal/target/_common/cc26xx\" --include_path=\"C:/ti/simplelink/ble_cc26xx_2_01_01_44627/Components/hal/include\" --include_path=\"C:/ti/simplelink/ble_cc26xx_2_01_01_44627/Components/osal/include\" --include_path=\"C:/ti/simplelink/ble_cc26xx_2_01_01_44627/Components/services/sdata\" --include_path=\"C:/ti/simplelink/ble_cc26xx_2_01_01_44627/Components/services/saddr\" --include_path=\"C:/ti/simplelink/ble_cc26xx_2_01_01_44627/Components/icall/include\" --include_path=\"C:/ti/simplelink/ble_cc26xx_2_01_01_44627/Components/icall/ports/tirtos\" --include_path=\"C:/ti/simplelink/ble_cc26xx_2_01_01_44627/Components/ble/include\" --include_path=\"C:/ti/tirtos_simplelink_2_13_00_06/products/cc26xxware_2_21_01_15600\" --include_path=\"C:/ti/simplelink/ble_cc26xx_2_01_01_44627/Projects/ble/SensorTag/CC26xx/Source/Application/Board_patch/interfaces\" --include_path=\"C:/ti/simplelink/ble_cc26xx_2_01_01_44627/Projects/ble/SensorTag/CC26xx/Source/Application/Board_patch/devices\" --include_path=\"C:/ti/simplelink/ble_cc26xx_2_01_01_44627/Projects/ble/SensorTag/CC26xx/Source/Application/Board_patch/CC26XXST_0120\" --define=POWER_SAVING --define=GATT_TI_UUID_128_BIT --define=FEATURE_REGISTER_SERVICE --define=FEATURE_OAD --define=FACTORY_IMAGE --define=USE_ICALL --define=TI_DRIVERS_PIN_INCLUDED --define=TI_DRIVERS_I2C_INCLUDED --define=TI_DRIVERS_SPI_INCLUDED --define=GAPROLE_TASK_STACK_SIZE=550 --define=HEAPMGR_SIZE=2872 --define=ICALL_MAX_NUM_TASKS=8 --define=ICALL_MAX_NUM_ENTITIES=11 --define=xdc_runtime_Assert_DISABLE_ALL --define=xdc_runtime_Log_DISABLE_ALL --define=CC26XXWARE --define=CC26XX --diag_wrap=off --diag_suppress=48 --display_error_number --diag_warning=225 --gen_func_subsections=on " "C:/ti/simplelink/ble_cc26xx_2_01_01_44627/Projects/ble/SensorTag/CC26xx/CCS/Config/appBLE.cfg"
making package.mak (because of config.bld) ...
configuring appBLE.xem3 from package/cfg/appBLE_pem3.cfg ...
generating custom ROM library makefile ...
Starting build of library sources ...
making C:/ti/simplelink/ble_cc26xx_2_01_01_44627/Projects/ble/SensorTag/CC26xx/CCS/Config/src/sysbios/sysbios.aem3 ...
gmake[1]: Entering directory `C:/ti/simplelink/ble_cc26xx_2_01_01_44627/Projects/ble/SensorTag/CC26xx/CCS/Config/src/sysbios'
Preprocessing library source files ...
Creating the SYS/BIOS library that contains the APIs not included in the ROM ...
0 [main] sh 6564 sync_with_child: child 9636(0x1DC) died before initialization with status code 0xC0000142
32 [main] sh 6564 sync_with_child: *** child state waiting for longjmp
C:/Users/TEJASD~1/AppData/Local/Temp/make15736-1.sh: fork: Resource temporarily unavailable
gmake[1]: *** [mangled__BIOS_lib.obj] Error 128
gmake[1]: Leaving directory `C:/ti/simplelink/ble_cc26xx_2_01_01_44627/Projects/ble/SensorTag/CC26xx/CCS/Config/src/sysbios'
gmake: *** [C:/ti/simplelink/ble_cc26xx_2_01_01_44627/Projects/ble/SensorTag/CC26xx/CCS/Config/src/sysbios/sysbios.aem3] Error 2
Build of libraries failed.
error: xdc.cfg.SourceDir: "C:/ti/xdctools_3_31_01_33_core/packages/xdc/cfg/SourceDir.xs", line 209: xdc.cfg.SourceDir : Build of generated source libraries failed: exit status = 2:
js: "C:/ti/xdctools_3_31_01_33_core/packages/xdc/cfg/Main.xs", line 160: Error: Configuration failed!
gmake.exe: *** [package/cfg/appBLE_pem3.xdl] Error 1
gmake.exe: *** Deleting file `package/cfg/appBLE_pem3.xdl'
gmake.exe: *** [package/cfg/appBLE_pem3.xdl] Deleting file `package/cfg/appBLE_pem3.h'
gmake.exe: *** [package/cfg/appBLE_pem3.xdl] Deleting file `package/cfg/appBLE_pem3.c'
js: "C:/ti/xdctools_3_31_01_33_core/packages/xdc/tools/Cmdr.xs", line 51: Error: xdc.tools.configuro: configuration failed due to earlier errors (status = 2); 'linker.cmd' deleted.
gmake: *** [configPkg/linker.cmd] Error 1
gmake: Target `all' not remade because of errors.
**** Build Finished ****
And error shown is
Description Resource Path Location Type
xdc.cfg.SourceDir: "C:/ti/xdctools_3_31_01_33_core/packages/xdc/cfg/SourceDir.xs", line 209: xdc.cfg.SourceDir : Build of generated source libraries failed: exit status = 2: appBLE.cfg /SensorTag/TOOLS C/C++ Problem
And appBLE.cfg file is
I have tried by changing ccs versions to 6.1.1 and 6.1.3. Also changed ble stacks as 2.0.0.42893 , 2.1.0.44423, 2.1.1.44627, 2.2.0.31. changed compilers 5.2.5 and 5.2.7. Even changed XDC 3.31.00.24, 3.31.01.33, 3.32.00.06. I changed TI RTOS versions also 2.13 , 2.11 , 2.18 , 2.20.
All of the above has been tried with combinations as per requirements of the respective version. But every time got errors. and error mentioned is repeated almost every time.(except power management issue occurred due to changing rtos versions from 2.13 to 2.18/2.20)
And I have uninstalled all the possible tools and extensions and deleted all the folders of texas instruments and ti with ccleaner before installing. And this process has been repeated for several times. But every time building is failed. I referred the discussions but nothing is working. And I had taken precaution about antivirus during installation. Even i checked by changing the workspaces and their locations and installing the CCS and other tools in other drive.
Please help me I have wasted more than 7 days due to this issue.
Thanks in advance.
Tejas Dighe60 said:0 [main] sh 6564 sync_with_child: child 9636(0x1DC) died before initialization with status code 0xC0000142
32 [main] sh 6564 sync_with_child: *** child state waiting for longjmp
C:/Users/TEJASD~1/AppData/Local/Temp/make15736-1.sh: fork: Resource temporarily unavailable
gmake[1]: *** [mangled__BIOS_lib.obj] Error 128
gmake[1]: Leaving directory `C:/ti/simplelink/ble_cc26xx_2_01_01_44627/Projects/ble/SensorTag/CC26xx/CCS/Config/src/sysbios'
gmake: *** [C:/ti/simplelink/ble_cc26xx_2_01_01_44627/Projects/ble/SensorTag/CC26xx/CCS/Config/src/sysbios/sysbios.aem3] Error 2
Build of libraries failed.
error: xdc.cfg.SourceDir: "C:/ti/xdctools_3_31_01_33_core/packages/xdc/cfg/SourceDir.xs", line 209: xdc.cfg.SourceDir : Build of generated source libraries failed: ex
One common reason for this error is having spaces or non-ASCII characters in the workspace path or any of the software tools paths. Please see this wiki:
tejasD said:As you suggested I changed user name to remove non ascii symbols. But it didn't work out.
Did you also check the second point in the link I sent:
" Take a close look at the CCS build console and ensure that the sh.exe used for the build is the one from the CCS directory. Also check your system PATH variable and
see if there is another sh.exe (or gmake.exe) in your system PATH earlier than the one from the CCS installation. These could also be part of other tools like cygwin or
WinAVR. If there is one, then that will be used for the build and could cause build errors such as this. In this case, remove those conflicting tools from the system PATH
or modify the PATH so that the sh.exe and gmake.exe from CCS are seen first."
There is a related thread here where having WinAVR in the system PATH resulted in a similar error.
Keil and Proteus do not harm CCS as per my experience.
But yes you can check whether your xdctool and ble stack versions are compatible with each other. It is solved by only trial and error method.
Try to uninstall each tool,stack and finally CCS. And use CCleaner for cleaning ti folder from C drive.
Try above method and if not worked then try to install ccs and stack in some other drive.
Hi all...
I also got same problem but it is solved by uninstalling the WinAVR and now code composer studio working fine. Before uninstalling of WinAVR I have got the error that the application was unable to start correctly(0x0000141).
Now it is solved!