This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Sir,
I am Vijay, While installing CCS 6.1.3.00034 on my lapy Windows 7 64-bit, I am getting the error message as mentioned below.
An error has occured. See the log file
C:\Users\name\APPData\Local\Temp\ccs_d26980a2-144f-4964-4a62-488c8d7bf5f0\workspace\.metadata\.log.
After Installation another error message as
1. An internal error occurred during: "CrashTrackerJob".
Could not initialize class com.ti.utility.filesystem.DirectoryService$SingletonHolder
2. An internal error occurred during: "License Acquisition". C:\ti\ccsv6\ccs_base\DebugServer\bin\LibraryLoader.dll: %1 is not a valid Win32 application
3. An internal error occurred during: "Loading device information". Could not initialize class com.ti.utility.filesystem.DirectoryService$SingletonHolder.
Please Guide.
Thanking You.
You may also be running into problems with windows patches not being up to date.
Please run the following command:
WMIC QFE|find "KB2999226"
It should return information on the patch. If it returns nothing, you're missing that update. You could get it by downloading from here: https://www.microsoft.com/en-us/download/confirmation.aspx?id=49093 or doing a windows update.
Danish