This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Error when running the cl6x >> ERROR: cannot run acp6x - invalid argument mode



Hi,

While trying to set my vector cast environment to do structural coverage. I'm finding that  cl6x cannot be called directly, even though the path is set. That  is, I need to prepend the complete tool path to the cl6x compiler command to get it to work look below. Is there a way to get around this, some system environment setting, or an option ?

( Here is an easy example)

C:\VCAST\Environments\main>path
PATH=C:\ProgramData\Oracle\Java\javapath;C:\Program Files (x86)\Serena\vm\win32\bin;C:\Program Files (x86)\Serena\vm\commo
2;C:\Program Files\Common Files\Microsoft Shared\Microsoft Online Services;C:\Program Files (x86)\Common Files\Microsoft S
osoft Online Services;C:\windows\system32;C:\windows;C:\windows\System32\Wbem;C:\windows\System32\WindowsPowerShell\v1.0\;
Files (x86)\Common Files\Roxio Shared\DLLShared\;C:\Program Files (x86)\Common Files\Roxio Shared\OEM\DLLShared\;C:\Progr
x86)\Common Files\Roxio Shared\OEM\DLLShared\;C:\Program Files (x86)\Common Files\Roxio Shared\OEM\12.0\DLLShared\;C:\Prog
(x86)\Roxio\OEM\AudioCore\;C:\DDC-I;C:\Program Files\Mercurial\;C:\Program Files\TortoiseSVN\bin;C:\Program Files\Tortoise
ram Files\TortoiseHg\;C:\ti\ccsv5\tools\compiler\c6000_7.4.13\bin;C:\ti\ccsv5\ccs_base\scripting\examples\loadti

THIS WAY IT DOES NOT WORKS

C:\VCAST\Environments\main>cl6x -mv6700 --abi=coffabi -Ooff -g main.c
>> ERROR: cannot run acp6x - invalid argument mode

C:\VCAST\Environments\main>dir
Volume in drive C has no label.
Volume Serial Number is F45E-275B

Directory of C:\VCAST\Environments\main

09/20/2016 04:46 PM <DIR> .
09/20/2016 04:46 PM <DIR> ..
09/15/2016 03:31 PM 49 main.c
1 File(s) 49 bytes
2 Dir(s) 292,449,701,888 bytes free

THIS WAY IT WORKS

C:\VCAST\Environments\main>C:\ti\ccsv5\tools\compiler\c6000_7.4.13\bin\cl6x -mv6700 --abi=coffabi -Ooff -g main.c

C:\VCAST\Environments\main>dir
Volume in drive C has no label.
Volume Serial Number is F45E-275B

Directory of C:\VCAST\Environments\main

09/20/2016 04:49 PM <DIR> .
09/20/2016 04:49 PM <DIR> ..
09/15/2016 03:31 PM 49 main.c
09/20/2016 04:49 PM 3,284 main.obj
2 File(s) 3,333 bytes
2 Dir(s) 292,449,697,792 bytes free

------

C:\VCAST\Environments\main>type main.c
/*
* main.c
*/
int main(void) {

return 0;
}