Other Parts Discussed in Thread: MSP-EXP430FR5739,
Tool/software: Code Composer Studio
Hi, guys!
We've recently upgraded the PCs in our university lab with Windows 10, 32-bit. I have entire course built on MSP-EXP430FR5739 board and now I experience terrible problems with the USB FET drivers.
When I try to debug my program first I get:
MSP430: Error initializing emulator: Could not find MSP-FET430UIF on specified COM port.
I go to the Project -> Properties -> General and I try to select from the drop-down menu "Connection" [TI MSP430 USB2] or [TI MSP430 USB3]. But then I get the error:
MSP430: Error initializing emulator: Tried to initialize USB FET number 2, but only found 1 USB FETs
I have a physical RS-232, I have no problems in the device manager, I see the MSP430 virtual COM (and it works fine). I have IAR for MSP430 also installed on the machines (also doesn't work). My CCS version is 6.2.0.00050.
Funny thing I noticed - If I use [TI MSP430 USB1] and if I start a Tera Term on the MSP430's virtual COM port WHILE the debugger is starting it succeeds.
Any help is appreciated!
Assistant L. Bogdanov
TU-Sofia
Bulgaria