Hi,
A problem remains, a variant for the debugging in the Ram is not translated.
I held 2 build configurations, one for FLASH, and one for RAM, this for debugging!
I checked now all the settings between FLASH and RAM, they are nearly the same, apart from optimization and of course a different cmd-file.
Now I can build with FLASH configuration, but it will not start with RAM configuration.
THe error message is:
"Errors occurred during the build. Errors running builder 'CDT Builder' on project 'VVK1'. java.lang.NullPointerException"
In the cosole this appears:
**** Clean-only build of configuration F2833x_RAM for project VVK1 ****
"C:\\ti\\ccsv6\\utils\\bin\\gmake" -k clean
gmake: *** No rule to make target 'clean'.
**** Build Finished ****
Any idea?
br Ralf