Part Number: RM44L520
Tool/software: Code Composer Studio
Hi,
Customer is developing SW on their custom board with RM44L520 on the board. They are using Segger debuggers on all of their MCU development and would like to use those here as well.
But when trying to debug/download from CCS with Segger, data verification error will occur:
CortexR4: GEL Output: Memory Map Setup for Flash @ Address 0x0CortexR4: File Loader: Verification failed: Values at address 0x00000022 do not match Please verify target memory and memory map.
CortexR4: GEL: File: C:\Users\nkarkkai\workspace_v7\test\Debug\test.out: a data verification error occurred, file load failed.
Interesting point is that if you select RM46 as a part in target configuration file, then this error does not occur. Also same debugger with IAR works well with RM44, but customer would like to use CCS instead for this project.
What could be the issue here that CCS/Segger combination does not seem to support correctly RM44?