Part Number: XDS560TRACE
Tool/software: Code Composer Studio
I'm having trouble connecting to my Blackhawk XDS560v2 after updating to the latest version of Blackhawk CCSv6.2 Emulation Update.
I'm currently running CCSv7.2.0.201705101800 on Window 10 64-bit.
Device Manager Output
Windows cannot verify the digital signature for the drivers required for this device. A recent hardware or software change might have installed a file that is signed incorrectly or damaged, or that might be malicious software from an unknown source. (Code 52)
The output of the test connection dialog:
[Start: Blackhawk XDS560v2-USB System Trace Emulator_0]
Execute the command:
%ccs_base%/common/uscif/dbgjtag.exe -f %boarddatafile% -rv -o -F inform,logfile=yes -S pathlength -S integrity
[Result]
-----[Print the board config pathname(s)]------------------------------------
C:\Users\jwr41\AppData\Local\TEXASI~1\CCS\
ti\0\0\BrdDat\testBoard.dat
-----[Print the reset-command software log-file]-----------------------------
This utility has selected a 560/2xx-class product.
This utility will load the program 'bh560v2u.out'.
E_RPCENV_IO_ERROR(-6) No connection: emulator was not found
Download failed for file C:\ti\ccsv7\ccs_base\common\uscif\xds560v2.out
An error occurred while soft opening the controller.
-----[An error has occurred and this utility has aborted]--------------------
This error is generated by TI's USCIF driver or utilities.
The value is '-250' (0xffffff06).
The title is 'SC_ERR_ECOM_EMUNAME'.
The explanation is:
An attempt to access the debug probe via USCIF ECOM has failed.
[End: Blackhawk XDS560v2-USB System Trace Emulator_0]
Any help would be appreciated. Thank you