Part Number: STARTERWARE-SITARA
Tool/software: Code Composer Studio
I'm trying to build the uartEcho project from C:\ti\AM335X_StarterWare_02_00_01_01\build\armv7a\cgt_ccs\am335x\evmAM335x\uart directory and I'm receiving a build error when the program is trying to run mkhex4bin.exe.
The Error message I'm receiving is
**** Build of configuration Debug for project uartEcho ****
"C:\\ti\\ccsv7\\utils\\bin\\gmake" -k -j 8 -s all -O
'Building file: C:/ti/AM335X_StarterWare_02_00_01_01/examples/evmAM335x/uart/uartEcho.c'
'Invoking: ARM Compiler'
'Finished building: C:/ti/AM335X_StarterWare_02_00_01_01/examples/evmAM335x/uart/uartEcho.c'
' '
'Building target: C:/ti/binary/armv7a/cgt_ccs/am335x/evmAM335x/uart/Debug/uartEcho.out'
'Invoking: ARM Linker'
<Linking>
warning: creating output section ".text" without a SECTIONS specification
warning: creating output section ".const" without a SECTIONS specification
warning: creating output section ".data" without a SECTIONS specification
warning: creating output section ".bss" without a SECTIONS specification
warning: creating ".stack" section with default size of 0x800; use the -stack
option to change the default size
'Finished building target: C:/ti/binary/armv7a/cgt_ccs/am335x/evmAM335x/uart/Debug/uartEcho.out'
' '
"C:/ti/ccsv7/utils/tiobj2bin/mkhex4bin.exe" failure occurred. Giving up.
' '
error: failed to read
"../../../../../../../binary/armv7a/cgt_ccs/am335x/evmAM335x/uart/Debug/uart
Echo.out"
Use of uninitialized value $str in pattern match (m//) at XML_TI_OFD.pm line 2146.
Use of uninitialized value $targ_num in hash element at XML_TI_OFD.pm line 1325.
Unexpected target: unknown at script/mkhex4bin.pl line 270.
The system cannot find the path specified.
**** Build Finished ****
uartEcho.out is being built but it looks like the mkhex4bin.exe can't find it. uartEcho.out is being stored to:
C:\ti\binary\armv7a\cgt_ccs\am335x\evmAM335x\uart\Debug.