Part Number: MSP430F5329
Tool/software: Code Composer Studio
Hi,
I am migrating a project. I got easily with the porting of some libraries but now I am facing a weird issue. The libraries are added on the include file and also precompiled (don't think this is necessary but I am desperate). When I try to compile it shows the functions which are not resolved but when I click them and then "Open Declaration" it will show where the functions are.
I find it odd because I assume that if the compiler knows where the function is it should resolve its name likewise.
As you can guess from the image the files with the symbols definitions is GPIO.c.
Thanks for your help