Other Parts Discussed in Thread: UNIFLASH, CC3220SF,
Tool/software: Code Composer Studio
Hi,
I'm trying to get a handle on the CC3220 development board. I've been able to build, run and debug the FreeRTOS demo application (simply_blinky variant) using CCS 8. I'd like to permanently program the board with that image but I am unsure how to move from the *.out file to... well whatever it is that UniFlash requires. I attempted enabling the HEX tool in CCS and was able to generate a single hex file, but either Uniflash rejected the file, or the "image" is unusable. My *.out file (ELF? Haven't checked yet) is ~500Kb but the hex file from the hex tool is only 98Kb. I contacted customer support and received the standard RTFM answer I expected. I was sent the UniFlash manual that really has nothing about what I am asking (other than it specifies what formats are accepted). In fact, the screens shown in processors.wiki.ti.com/index.php/UniFlash_v4_Quick_Guide look nothing like the UniFlash tool that I have installed.
The only image I am able to flash is the OOB example imported from the pre-compiled zip file. This 'project' contains a mcuflash.img and a service pack BIN file. I have neither of these for my FREERTOS executable. I am no closer to a solution.
Is there any documentation on 'transferring' executables from CCS to a Uniflash image? Perhaps I am simply way out in 'left field' and have missed something?