Part Number: CC3220
Tool/software: Code Composer Studio
Hi,
I'm trying to set up uniflash to automate a few things with the image creator and cc3220, I encountered a few issues.
Corrupted project
Sometimes I get the error: "Error loading users files: File paths must not start or end with "/". "
The only thing I can do afterwards is to recreate or reimport the exact same project to make it work. I'm not sure how to reproduce it but it happens up to a few times per day, always when coming back to it after working on something else.
Is there a known issue with this?
Shortcut to start directly in image creator
Is there a way to start directly image creator for cc3220 without having to use the window "Choose Your Device" ?
Dev mode in command line
How can I set up the project to be in development or production mode using the command line?
I expected to be able to run something like:
SLImageCreator.exe project --name Sensor_v2 --reconfig dev_mode.json
With the json being:
"Simplelink":
{
"devMac": "58:7a:62:41:47:80"
}
I've tried a few permutations with "reconfig", "reconfigure", as well as with and without "--file" but always get a command line parsing error.
MCU image replace in GUI
When I use the advanced=>UserFile=>Overwrite file, I get the error "Error: MCU image file exceeds the maximum size for this device".
The only way I found is to delete the file, and reupload it and respecify the certificate and private key, which is a pain when doing it often...
I cannot use simple mode since this overwrite the certificate store.
Is there another way? Or is it possible to fix this in the next versions?
Note: I'm using uniflash 4.5
P.S. Is it the correct forum for uniflash?