Other Parts Discussed in Thread: CC2652R
Tool/software: Code Composer Studio
Hi,
I wanted to display English and Spanish in my project which uses the cc2652R and the ST7735S Display Controller. For the purpose I downloaded the TivaWare SDK and then obtained the ftrasterize tool from there.
Then I downloaded a font that supports both English and Spanish.( ASCII characters from 32 to 256). Then I generated the font.c file using ftrasterize using the following command on cmd prompt :
"ftrasterize.exe -f font -s 24 -e 255 font.ttf". This gave me a font file with Graphics_FontEx type ( since it was upto 256)
Then I included the font.c file obtained to my project and set the font to the corresponding. Then as per the following post from Steffen Fuchs: https://e2e.ti.com/support/microcontrollers/msp430/f/166/t/664949?tisearch=e2e-quicksearch&keymatch=above%20127
I had used the string draw functions changing int8_t to uint8_t. Then tried using those functions to display the Spanish characters. However when I tried to do so, either the data was not appearing at all or some other character was appearing in place of the given character.
Is there any other step to be done ?
Regards,
Shyam