Part Number: CC1352R
Tool/software: Code Composer Studio
It used to be that you could create a pre-defined symbol like so:
Then, when you build, you get a --define=QX_008_752_T_HANDLE, which can be used to ifdef things in and out. This still works fine. What doesn't work is the IDE showing which code blocks are compiled in vs out. That feature doesn't work when you do this.
If you then add "QX_008_752_T_HANDLE" to the list of pre-defined symbols directly, it works for the build, and the editor features then work. Having this work is great when managing a larger number of similar builds.
This used to work correctly in CCS 8.2, stopped working in 8.3, and continues to not work in CCS 9.0