Part Number: CCSTUDIO-C2000
Tool/software: Code Composer Studio
Hi,
I want to ask a question similar to this thread with regards to debugging C2000 cores in CCS: https://e2e.ti.com/support/tools/ccs/f/81/t/809381?tisearch=e2e-quicksearch&keymatch=C2000%20real-time%20debug
My company is currently using F28M35 concerto devices and I have been a user of C2000 for a few years. I do a lot of control development and one important desired feature is plotting uC internal variables at control bandwidth (say a few kHz). With ARM Cortex M cores, this can be done with background memory access so if a debugger is powerful enough, you can turn every cortex M into a small o-scope.
My experience with C2000 has been that it's very difficult to achieve such functionality. The continuous refresh in CCS is about 1 - 10Hz so the usefulness is very limited. I have also tried setting up breakpoints and configure the property of the breakpoints to be "update all windows" and it seems it's too intrusive to the application control loop.
My question is what technique/tool can I use to view C2000 internal variable values at high refresh rate through the debugging interface? Reading about the XDS100/200/560 debuggers did not give me the impression that what I'm asking is possible. So far I have implemented software circular buffers to capture the values and then later transfer those values to a csv for post-processing. But this is very time-consuming and non-intuitive. I feel like TI must have thought about this since C2000 is control-oriented.