Tool/software: TI C/C++ Compiler
Dear All,
We are migrating from our old CPU TMS320C3x to latest ARM® Cortex™-A9 based CPU, while porting the code we see compilation issues due to incompatibility with
arm-none-eabi-gcc (GCC) 8.2.0
Copyright (C) 2018 Free Software Foundation, Inc.
I would like to bring one such scenario here, the below code snippet works with ti provided compiler
#include <stdio.h>
#define MYVAL51 51
#define GET_MY_VAL(val) MYVAL##val
#define GET_MY_VAL_HEX(val) 0x##val
void main(){
printf("Hello\n");
printf("Value = %d\n", GET_MY_VAL(51));
printf("Value in hex = %x\n", GET_MY_VAL_HEX(GET_MY_VAL(51)));
}
but failing with below error when used with arm-none-eabi-gcc (GCC) 8.2.0, following is the error
pre_pro.c: In function 'main':
pre_pro.c:5:29: error: invalid suffix "xGET_MY_VAL" on integer constant
#define GET_MY_VAL_HEX(val) 0x##val
^~
pre_pro.c:9:32: note: in expansion of macro 'GET_MY_VAL_HEX'
printf("Value in hex = %x\n", GET_MY_VAL_HEX(GET_MY_VAL(51)));
Please help to address the above issue. (I have a workaround though, that is modify MYVAL51 as 0x51) but I am looking from compiler options standpoint.
Thanks in advance!
Regards,
Vamshi G.