Hi everybody,
I am using CCS 4.2 and have a project using DSP/BIOS 5.41. It is compiled for a C64+ DSP.
The project is named "core" and its source files are located in a directory "core". The CCS4-project files are located in a subdirectory "core/ccs4". There are several configurations like "Debug" and "Release". The DSP/BIOS configuration (core/core.tcf) is linked to the project.
If I build the project with configuration "Debug", then the generated files corecfg.cmd, corecfg.h... are put in the directory core/ccs4/Debug. But since corecfg.h is included also from other dependent projects, I would like to put them into another directory which is the same for each configuration, e.g. with the core.tcf in the core directory.
So I added the entry -Dconfig.programName="<src_dir>/core" in the Build Settings of the TConf Script Compiler. But this leads to errors like
'Building file: corecfg.s??'
'Invoking: Compiler'
"C:/Programme/Texas Instruments/ccsv4/tools/compiler/C6000 Code Generation Tools 6.1.19/bin/cl6x" -@"corecfg_ccsCompiler.opt"
>> ERROR: no source files, nothing to do
'Finished building: corecfg.s??'
' '
'Building file: corecfg_c.c'
'Invoking: Compiler'
"C:/Programme/Texas Instruments/ccsv4/tools/compiler/C6000 Code Generation Tools 6.1.19/bin/cl6x" -@"corecfg_c_ccsCompiler.opt"
>> ERROR: no source files, nothing to do
'Finished building: corecfg_c.c'
and
cannot find file "<src_dir>/Core/DspObj/Debug/corecfg_c.obj"
cannot find file "<src_dir>/Core/DspObj/Debug/corecfg.obj"
and many other linker errors.
Is it possible to put the generated files in another directory as it is described for CCS 3.3 (http://processors.wiki.ti.com/index.php/DSP_BIOS_FAQ#Q:_Is_it_possible_to_change_the_default_directories_for_the_BIOS_generated_files.3F)?
If yes, what am I doing wrong?
Thanks,
Tobias