Part Number: PROCESSOR-SDK-DRA8X-TDA4X
Tool/software: Code Composer Studio
Hi,
I am really new to the TI ecosystem and i would like to know the following details regarding the Jacinto 7 Platform. Pardon me if they are too basic ideas. I have tried to read the documentation but i felt it to be a little bit confusing.
1. How do I deploy a Deep learning application onto a TDA4 core ? Is it through CCS or is there any other software / module needed? How to setup TI-RTOS on the RTOS core ( via sd card or any other means) ?
2. How to get access to the TI emulator for Jacinto 7 ?
3. Is there a way to modify the packages installed on Linux core on Jacinto 7 like we usually do on Linux using apt / apt-get ? Can i use a monitor / Keyboard / mouse to interact with the Jacinto 7 Linux core? or can I use SSH to communicate with it from host machine?
4. Is there any chance to use a low level micro-controller like arduino with the Jacinto 7 linux core for robotic applications such as implementing a motion controller ?
5. How can i enable using the Linux core and RTOS core together.
a. How to enable message passing between RTOS and Linux cores ( applications)?
b. Is there a way to use USB camera's with RTOS on Jacinto 7 board ? The demo's on internet shows onloy the camera's supported on Fusion daughter boards. ?
c. is there a chance to get Robot Operating System up and running on either of the RTOS / arm core ? Does the RTOS support micro-ROS ?4.