This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
Hello, I am trying to charge a code into a uC TMS570LS0714 using JTAG connection through XDS110 debug probe. I am using the CTI-20 pins connectors as shown in the figure. I show you the configuration I am using as well in the figures. The pinout configuration is the following one:
uC pin XDS CTI-20 pin
TMS-108 SWDIO/TMS-1
nTRST-109 NTRST-2
TDI-110 TDI-3
TDO-111 SWO/TDO-7
TCK-112 TCK-11
RTCK-113 NONE
3.3 V VTRef-5
GND GND-10
The error I have trying to debug and charge the code on the uC is:
Error connecting to the target:
(Error -2131 @ 0x0)
Unable to access device register. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK).
In addition, trying the test connection I get this error:
This error is generated by TI's USCIF driver or utilities.
The value is '-233' (0xffffff17).
The title is 'SC_ERR_PATH_BROKEN'.
The explanation is:
The JTAG IR and DR scan-paths cannot circulate bits, they may be broken.
An attempt to scan the JTAG scan-path has failed.
The target's JTAG scan-path appears to be broken
with a stuck-at-ones or stuck-at-zero fault.
I have checked all the connections and I am powering the XDS debug probe with 3.3V on one side and my target with 6.5 V but thanks to dome DC/DC converters I have 3.3 and 1.2 V for the uC.
I tried with a slower JTAG speed at 1 MHz but the problem is the same, I will try tomorrow to shorten the cables but I have a problem even just to recognize the debugger without JTAG connection. So could be another problem?
trying the test connection I get this error:
This error is generated by TI's USCIF driver or utilities.
The value is '-233' (0xffffff17).
The title is 'SC_ERR_PATH_BROKEN'.
The explanation is:
The JTAG IR and DR scan-paths cannot circulate bits, they may be broken.
An attempt to scan the JTAG scan-path has failed.
The target's JTAG scan-path appears to be broken
with a stuck-at-ones or stuck-at-zero fault.
I am trying to charge a "hello world" program on a launchpad TMS570LS12x development kit as well. In this case, I am using the xds110 debugger to power supply the target, and the launchpad has some pins to connect a JTAG, so I connected everything but I have the same problems even just testing the connection. Is there some way to test just the XDS110 debug probe?
[Start: Texas Instruments XDS110 USB Debug Probe_0]
Execute the command:
%ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -S integrity
[Result]
-----[Print the board config pathname(s)]------------------------------------
C:\Users\Andrea\AppData\Local\Texas Instruments\
CCS\ccs1011\0\0\BrdDat\testBoard.dat
-----[Print the reset-command software log-file]-----------------------------
This utility has selected a 100- or 510-class product.
This utility will load the adapter 'jioxds110.dll'.
The library build date was 'May 7 2020'.
The library build time was '21:10:18'.
The library package version is '9.2.0.00002'.
The library component version is '35.35.0.0'.
The controller does not use a programmable FPGA.
The controller has a version number of '5' (0x00000005).
The controller has an insertion length of '0' (0x00000000).
This utility will attempt to reset the controller.
This utility has successfully reset the controller.
-----[Print the reset-command hardware log-file]-----------------------------
The scan-path will be reset by toggling the JTAG TRST signal.
The controller is the XDS110 with USB interface.
The link from controller to target is direct (without cable).
The software is configured for XDS110 features.
The controller cannot monitor the value on the EMU[0] pin.
The controller cannot monitor the value on the EMU[1] pin.
The controller cannot control the timing on output pins.
The controller cannot control the timing on input pins.
The scan-path link-delay has been set to exactly '0' (0x0000).
-----[An error has occurred and this utility has aborted]--------------------
This error is generated by TI's USCIF driver or utilities.
The value is '-233' (0xffffff17).
The title is 'SC_ERR_PATH_BROKEN'.
The explanation is:
The JTAG IR and DR scan-paths cannot circulate bits, they may be broken.
An attempt to scan the JTAG scan-path has failed.
The target's JTAG scan-path appears to be broken
with a stuck-at-ones or stuck-at-zero fault.
[End: Texas Instruments XDS110 USB Debug Probe_0]
Which value for the resistor? It will be not so easy as the PCS is done as shown in the previous picture. I will put the resistor directly in to the connector. In addition I would like to comment that I have tried with a TI lanchpad wich has almost the same microcontroller, the launchpad is the LAUNCHXL2-TMS57012
trying to charge a hello world code with the target configuration as shown in figure above, using the debugger into the lanchpad wich should be the same XDS110 and I have exactly the same problem doing the test connection and the debug. Could it be a software problem? maybe version of CCS? I am using the last 10.1.1.
I noticed there are 6 wires between JTAG emulator and your board? What are those signals?
JTAG signals of XDS110 header: TCK, TMS, TDI, TDO, nTRST, GND, Vref, RTCK
I am using on JTAG signals of XDS110 header 3.3 V for VTRef-5 and GND for GND-10 with a power supply. In addition:
uC pin XDS CTI-20 pin
TMS-108 SWDIO/TMS-1
nTRST-109 NTRST-2
TDI-110 TDI-3
TDO-111 SWO/TDO-7
TCK-112 TCK-11
RTCK-113 NONE
Hello,
Please share the GND between JTAG emulator and your board. The JTAG emulator needs to know the power supply (VTref, 3.3V) on your board.
Hello, I did but I have the same problem. In addition I have a launchpad with the same XDS110 debugger and a uC of the same family. The launchpad works correctly and I am comparing the test connection of the debug in both cases. The signal on the PCB are a bit dirty but the big difference is on the TDO. I show you the images below. The images ended in L are the Launchpad signals, the images ended in P are the PCB signals:
Oh, I didn't see it. So it should be pulled up to 3.3V or it could be pulled up to 1.2V? It is because I have a 1.2V signal on one side of this pin. Which resistor do you recommend me to use for this pull up? Can I connect this pin directly to the voltage without resisotr? In the datasheet as shown in table I can't see any resistor value.
nPORRST has to be pulled up to 3.3V (VCCIO).
2.2kohms is good enough.
Please refer to the nPORRST Electrical and Timing Requirements in datasheet (Table 6-4).
If your problem has been resolved, please click the "Solved" button. Thanks