This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
I can't reply, so I'll create the following continuation here.
subject
I write to TMS320F28375D with XDS110 with UniFlash and CCS, but I cannot write due to an error.
I manually updated the firmware, but it does not improve.
I connected the TI 14-pin JTAG Isolator and tried to write, and I was able to write and debug normally.
As improved reason, what will be considered?
user6507111 said:I connected the TI 14-pin JTAG Isolator and tried to write, and I was able to write and debug normally.
I am glad to hear that you were able to debug normally. The iso adapter may have provided a more stable connection with the custom board. I assume before that, the xds100 debug probe was connected directly to a 14-pin JTAG header on the board?
Thanks
ki
The xds100 / 200 debug probe was directly connected to the 14-pin JTAG header on the board.