This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Debug Server Scripting (DSS) generic loader 'loadti' caching of loaded objects



Hi,
using DSS (Debug Server Scripting) generic loader 'loadti' unit testing is performed in a Linux environment.
Consecutive automation tests are performed sequentially.

Often Java "Segmentation fault" occurs at some point, mostly after several preceeding 'loadti'-loaded tests performed well.
Once the failure occurs, it remains there at the same test (even on test-repetition).

  • testEnv.outFiles: ____.out
    Loading ____.out
    #
    # An unexpected error has been detected by Java Runtime Environment:
    #
    #  SIGBUS (0x7) at pc=0xf7e484fc, pid=46945, tid=2916301680
    #
    # Java VM: Java HotSpot(TM) Server VM (11.3-b02 mixed mode linux-x86)
    # Problematic frame:
    # C  [libc.so.6+0x1384fc]

Java that is in use is the one that comes with CCS5.5:  java version "1.6.0_13"

We have already discovered the cause for that behaviour:

  • 'loadti' caches loaded .out files in the following folder: /dev/shm/
    After tests get performed and 'loadtti' terminates, most of the cached objects remain in this as
    'OFS_outname.out_53394'
  • With a time this amount of data gets too large causing the Java error.
    Manual emptying this folder helps.

Finally the question:

  • How is it possible to control what happens with the content of the folder /dev/shm/ ?

Thanks.

  • Hello,

    That is interesting, I have not seen this issue before. I also do not see the *out files getting cached in the /dev/shm/ directory. However I used a more recent version of CCS. I'll need to try with CCSV5.5.

    Also, what Linux distro (and version) are you using?

    Thanks

    ki

  • Hello,
    the issue is observed on this machine (test server):

    • Red Hat Ent. Linux Server release 6.10 (Santiago)

    thanks to DSS-usage in docker container which (as object trash grows) runs out of memory.
    It is annoying to always have take care of size of object-trash in /dev/shm/ (by emptying it or others).

    By the way, DSS is used also on various workstations:

    • Red Hat Ent. Linux Server release 6.40 or newer versions 7

    Here workstation do not easily run out of memory, so Java "Segmentation fault" doesn't appear. However, the DSS object trash can be found in the folder /dev/shm/ as well. Trash-files (cached objects) are named according to the same pattern:
    OFS_<modulname>.out_53394

    I do not think an issue has anything to do with operating system (Linux), but DSS Java scripting behind it.

    Thanks,

    MladenS

  • I see the behavior when I run loadti with my CCSv5.5 installation. It looks like something that the CCS did with older versions that since has changed. I'll need to see if there is a way to turn this off in CCSv5. But note that CCSv5.5 is very old and unsupported. Any reason you still need to use this version?

    Thanks

    ki

  • Here's the strong reason for still using CCSv5.5:
    It is the last CCS version coming with (cycle-accurate) DSP-simulator support.
    Thanks,
    MladenS

  • It appears that the issue is not scripting (or loadti) specific, but will occur when a program is loaded by the CCS debugger (whether via scripting or IDE). It also does not appear to happen with CCS versions 6.x or greater. I do not see an option to turn off this behavior in CCSv5. As a simple workaround, I would suggest creating a little script that will clear the folder and then call loadti.sh). This should have the same effect.

    ki

  • DSS is started using a (Bash) script like this:
    $DDS_PATH/dss.sh $LOADTI_PATH/main.js ...

    Manually applying a small (post-processing)cleaning-script is exactly what I do at the moment.
    I thought there might be a possibility in DSS-scripting itself (or its options) to control this.

    Thanks a lot for checking this!
    MladenS