TIDA-010057: Can I adjust the output voltage of high power side?

Part Number: TIDA-010057
Other Parts Discussed in Thread: AFE5832, TX7332, , LM3488

Hello TI experts,

My customer considers 4 x TX7332 and 2 x AFE5832 for their product.

they have to think about power tree, and I am going to suggest TIDA-010057.

and here are some questions,

1. in the guide document, positive/negative output voltage is up to +/-80V. can I adjust it to +/-100V?

if not, can you recommend other IC instead of LM3488?

2. what is the maximum current of this reference?

my customer wants over 3A for 4 x TX7332.

please check these issues. Thanks.

Best regards,

Chase