This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PMP40500: UNDER VOLTAGE LOCK OUT OF PMP40500

Part Number: PMP40500

Hi Team

Please tell me the UNDER VOLTAGE LOCK OUT OF PMP40500 

Best regards,
William

  • Hi, 

    The minimum input voltage is around 40Vin if just regulated output with no full load. Because the primary to secondary turn ratio is 1.5 and half bridge maximum duty cycle is around 48%. However, When 40Vin, the input RMS current of FET and transformer will be increasing. It can't support 40Vin 500W output considering FET an d transformer thermal.

    Thanks.