Other Parts Discussed in Thread: TPS23734EVM-094, TPS23754, TPS23734, TPS23730EVM-093
Dear Specialists,
My customer is considering PMP9563 as a reference.
They have a question about switching FET between PMP9563 and TPS23734EVM-094.
I would be grateful if you could advise.
---
The PMP9563 uses the FDS86242 as the switching FET.
On the other hand, the recommended FET of the new product TPS23734EVM-094 is FDMS86252.
The FDM86252 has a higher rated current and lower ON resistance, so I think it is a higher-end product.
The TPS23734 is a new device that supports up to IEEE 802.3b, but the PD power level is 13W and 25W, and there is no difference between the TPS23754 and PD power level.
What is the reason for using the higher performance FET (FDMS86252) in TPS23734?
Is there any problem to use FDS86242 for IEEE802.3at PD Class 4 (25.5W)
---
I appreciate your great help in advance.
Best regards,
Shinichi