Hi,
In the Altium Designer project file of TIDA-00623, there is a green circle on the M7 LPKF Text Top Layer. What is the M7 LPKF Text Top Layer used for? The screenshots as shown below.
Thanks.
Kind regards,
Evangeline
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
In the Altium Designer project file of TIDA-00623, there is a green circle on the M7 LPKF Text Top Layer. What is the M7 LPKF Text Top Layer used for? The screenshots as shown below.
Thanks.
Kind regards,
Evangeline
Hi Bill,
Thanks a lot.
Another Question here. I noticed that there is also an M7 LPKF Text Top layer in the project files of other reference designs. What is the layer M7 LPKF Text Top used for? In addition, what does LPKF mean?
Thanks.
Kind regard,
Evangeline
Hi Evangeline
M7 and M8 are not needed they are part of he standard pcb layout stack up.
Hi Bill
Thanks a lot. And how about LPKF? What is the full name of the acronym LPKF? And what does it mean?
Thanks.
I think it might not be used for laser de-paneling because laser de-paneling only needs one layer. Why does it need to use M7 Top and M8 Bottom two layers? Could you please check what LPKF means and its full name? Thanks.
Warm wishes at Thanksgiving!
Have you finished checking the meaning and the full name of LPKF?
Thanks.
The M7 and M8 layers are not needed for TIDA-00623 design.
I have checked with the layout teams and they are not using it. The layers are a standard part of the layout stack up template used for evaluation boards.
Layout team indicated it is to support LPKF Laser & Electronics PCB Depaneling and PCB Milling system (rapid prototyping).
So LPKF is the name of a company and the company has Laser Depaneling system and PCB Milling system, right?
So LPKF is the name of a company and the company has Laser Depaneling system and PCB Milling system, right?