We have asked before about Current Limitations of daughter cards
Thanks to Riccardo answer before
"the daughter board based on GaN technology is not able to reach 16 Arms because the current layout does not allow a higher switching speed. The maximum switching speed that we can achieve without no problem is 30 kV/us.
Currently, this issue is addressed and we are improving the layout by keeping the same device.
From the calculation that I made, we are going to be able to switch up to 100 kV/us with the new layout. This significant rising in the switching speed will allow the daughter board to work at 16 A operation."
We need to know what is the maximum current limit of the GaN Leg now while switching at " 30 kV/us ", and what is maximum current limit of SiC MOSFET Leg in the current layout?, does it have the same limitation regarding switching speed ?.