Other Parts Discussed in Thread: IWR1443,
We are developing a radar level transmitter using IWR1443 TIDEP-0091 for coal bunker measurement.
The coal bunker is 35 meters high. The radar level transmitter is mounted on the top of bunker.
We designed a PTFE lens for iwr1443. The diameter of the lens is 80mm, and focal length is 32mm, Beam width is 2.3° according to the simulation.
We increase profileCfg->rxGain from 44 default in DEMO_CONFIG100 to 52(or 116), but the ehco wave is very flat, no peak.
Are threre any software parameters to increase taget signal magnitude and decrease noise in solid measuring environment?