This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-00573: 3 phase motor current measurement using CT

Part Number: TIDA-00573

Hi, we are going to use TIDA 00573 to measure current of 3 phase motors, I wanted to clarify if we can use the same circuit to measure current up to 500A or not ?

Regards,

Atul