Part Number: PMP30763
Hi,
I went through the application note: https://www.ti.com/lit/ug/tidt169/tidt169.pdf?ts=1655221421024&ref_url=https%253A%252F%252Fwww.google.com%252F and on page 21 it states that for DO160, the harmonic limits are calculated based on the fundamental current at 96Vac but the testing has to be done at 115Vac. In my case, the power supply (PFC designed based on TI CCM PFC Chip) goes down to 90Vac (100-122Vac +/- 10%) at 400Hz. If I will calculate the fundamental based on this limit then I will have plenty of margin at the 115Vac.
Please confirm if this is the correct interpretation of the standard?
Regards,
Nitish